It is an international airport serving Hamburg, Germany. It originally covered 440,000 square meters. Since then, the site has grown more than tenfold to 5.7 square kilometers. The main apron covers 320,000 square meters. The airport is 8.5 km north of the centre of the City of Hamburg in the Fuhlsbüttel quarter. The Airport was opened in January 1911, it is the oldest Airport in Germany which is still in operation.
INSTALLATION: ...
CABLE FAMILY: Low Fire-Hazard
PLACE: Hamburg - Germany
BUILDING TYPE: Airport
MAP: see the map
<< previous application next application >>