Contacts  |  Turkish  |  Group Corporate Site  |  Search

  Turkey
Our Company
Energy Business
Telecom Business
Investor Relations
People & Careers
Home    Our Company: Press Area    ??? NavText ???    CasaLight™ Xtreme
A worldwide leading player
Knowledge, technology, solutions
Research & Development
Ethical code
History
Prysmian in Turkey
Certificates
Cable@Prysmian
Press Area
Corporate News
Logos

Prysmian Announces CasaLight™ Xtreme

The Leading Edge Of Bend Insensitive Optical Fibres

Prysmian announces the arrival of its latest innovation in bend optimized fibres, CasaLight™ Xtreme.  This fibre advances the CasaLight™ fibre family, already comprising of CasaLight™, and CasaLight™ Plus, far past the specifications of ITU G.657 A and B.  CasaLight™ Xtreme is targeted at the most demanding FTTH applications, where extreme bending radii are unavoidable. 

Prysmian customers now have a full spectrum of choices when dealing with FTTx installations. CasaLight™ is ideal when bending radii down to 10mm are encountered. This is commonly applied within the Riser columns. CasaLight™ Plus becomes essential in the horizontal cabling from the Riser shaft to the first point of presence into the customer premises, where the pathway would encounter bending radii down to 7.5 mm.

In the most demanding applications, CasaLight™ Xtreme provides the best solution by allowing bending radii down to 5mm. CasaLight™ Xtreme has been designed to withstand sharp 90 degree bends under tension and installation with staple guns when used in Prysmian specialty MDU cables.

As the name suggests, the fibre is intended only for use when extreme bend conditions are encountered. For most everyday installations the existing CasaLight™ family members are considered sufficient. Nevertheless it is essential to have CasaLight™ Xtreme available to cover the full range.

The segmentation of the CasaLight™ bend insensitive fibre family, allows customers to optimize the cost of their infrastructure by using the right fibre for the right application. CasaLight™, CasaLight™ Plus and CasaLight™ Xtreme also maintain full compatibility with standard equipment, connectors and fibre already installed in accordance with ITU Recommendation G.652.

Prysmian has continued to maintain its commitment to the environment with a fluorine free production process for CasaLight™ Xtreme as with all of its other fibre products.

CasaLight™ Xtreme optical fibre is now fully available in all of Prysmian's extensive range of FTTH cable products ensuring maximum levels of performance under the most demanding of installation scenarios.

Site Map  |  Legal Information  |   Company info  |  Copyright © 2012 All rights reserved.